This function refers to the memory.
[Specification format]
debugger.Memory.Read(address, memoryOption = MemoryOption.Byte)
|
[Argument(s)]
|
|
|
|
address
|
Specify the address to reference.
|
|
memoryOption
|
Specify the display unit.
The units that can be specified are shown below.
|
|
|
|
|
MemoryOption.Byte
|
Byte unit (8 bits) (default)
|
|
MemoryOption.HalfWord
|
Half-word unit (16 bits) [RH850,RX,V850]
|
|
MemoryOption.Word
|
Word unit (RL78,78K: 16 bits, RH850,RX,V850: 32 bits)
|
[Return value]
Referenced memory value (numeric value)
[Detailed description]
- | This function displays the address specified by address, according to memoryOption in hexadecimal format. |
- | When multiple values are to be read from consecutive addresses, using debugger.Memory.ReadRange reduces the overhead of processing for reading. |
[Example of use]
>>>debugger.Memory.Read(0x100)
0x10
>>>value = debugger.Memory.Read(0x100)
0x10
>>>print value
16
>>>debugger.Memory.Read(0x100, MemoryOption.HalfWord)
0x0010
>>>
|