Sets the clock source.
[Syntax]
#include "r_cg_macrodriver.h"
#include "r_cg_cgc.h"
MD_STATUS R_CGC_Set_ClockMode ( clock_mode_t mode );
[Argument(s)]
I/O |
Argument |
Description |
I |
clock_mode_t mode; |
Clock source type MAINCLK : Main clock oscillator SUBCLK : Sub-clock oscillator PLLCLK : PLL circuit HOCO : High-speed on-chip oscillator LOCO : Low-speed on-chip oscillator |
[Return value]
Macro |
Description |
MD_OK |
Normal completion |
MD_ERROR1 |
Exit with error (abend) |
MD_ARGERROR |
Invalid argument mode specification |