Clock generation circuit
Below is a list of API functions output by the Code Generator for clock generation circuit use.
Table 3.2 API Functions: [Clock Generation Circuit]
| 
       API Function Name  | 
    
       Function  | 
| 
       Performs initialization required to control the clock generation circuit.  | |
| 
       Performs user-defined initialization relating to the clock generation circuit.  | |
| 
       Performs processing in response to the osillation stop detection interrupt.  | |
| 
       Performs processing in response to the oscillation stop detection NMI.  | |
| 
       Sets the clock source.  |