Everything

r_riicn_receive_interrupt

Performs processing in response to the receive data full interrupts (RXI).

Remark         This API function is called to run interrupt processing for the receive data full interrupts (RXI).

 

[Syntax]

static void    r_riicn_receive_interrupt ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.