Everything

R_RIICn_StartCondition

Issues the start condition and causes a transfer error and an event generation interrupt (EEI).

Remark 1.      This API function is called as the internal function of R_RIICn_Master_Send and R_RIICn_Master_Receive.

Remark 2.      r_riicn_error_interrupt is called in response to calling of this API function.

 

[Syntax]

void    R_RIICn_StartCondition ( void );

Remark         n is the channel number.

 

[Argument(s)]

None.

 

[Return value]

None.