Issues the stop condition and causes a transfer error and an event generation interrupt (EEI).
Remark r_riicn_error_interrupt is called in response to calling of this API function.
[Syntax]
void R_RIICn_StopCondition ( void );
Remark n is the channel number.
[Argument(s)]
None.
[Return value]
None.