Everything

[Fixed-Sized Memory Pool] tab

This tab displays the fixed-sized memory pool information (e.g. Fixed-Sized Memory Pool Name and ID) of the RI78V4.
Figure A-16. [Fixed-Sized Memory Pool] Tab
The following items are explained here.
[How to open]
- From the [Debug] menu, select [Download].
- From the [View] menu, select [Realtime OS] >> [Resource Information].
[Description of each area]
(1) Information display area
(a) First layer
This layer displays the fixed-sized memory pool information (e.g. Fixed-Sized Memory Pool Name and ID) of the RI78V4.
This layer consists of the following items.
Fixed-Sized Memory Pool Name
An icon indicating the current status of the fixed-sized memory pool and the name of the fixed-sized memory pool are shown in the following format.
Icon Name
Note that if the name of the fixed-sized memory pool is undefined, the name will appear as "ID".
There are waiting tasks.
There are no waiting tasks.
ID
The ID of the fixed-sized memory pool is shown.
Queue Status
The current status of the fixed-sized memory pool is shown.
Waiting Tasks
There are waiting tasks.
Empty
There are no waiting tasks.
Top Address
The start address of the fixed-sized memory pool is shown.
Block Size
The size per block (in bytes) of the fixed-sized memory pool is shown.
Total Blocks
The block count of the fixed-sized memory pool is shown.
Free Blocks
The number of free memory blocks is shown.
Attribute
The task queuing method "TA_TFIFO" is shown.
TA_TFIFO
FIFO order

Remark If the fixed-sized memory pool information (e.g. Fixed-Sized Memory Pool Name and ID) in each cell is double clicked, then Memory panel displays the contents of the fixed-sized memory pool, and the caret moves to the corresponding location.
(b) Second layer
The waiting task information (e.g. Task Name and ID) only appears if there are tasks queued in the fixed-sized memory pool's wait queue.
See the [Task] tab for details about waiting task information.
Figure A-17. [Fixed-Sized Memory Pool] Tab (Waiting Task Information)
Remarks 1. If the waiting task information (Task Name, ID, Status, Wait Factor, Wait Data, Time Left, Interrupt, Current Priority, Task Start Address, Current PC) in each cell is double clicked, then Editor panel displays the source file of the task, and the caret moves to the corresponding location.
2. If the waiting task information (Current Task SP) in the cell is double clicked, then Memory panel displays the contents of the task stack, and the caret moves to the corresponding location.
[Context menu]
The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
(1) Header row
Display
Displays cascade menus for selecting the header items to display.
Selected item name
The following items are displayed for selection.
Fixed-Sized Memory Pool Name, ID, Queue Status, Top Address, Block Size, Total Blocks, Free Blocks, Attribute
Checked
The item in question will be displayed.
Not checked
The item in question will not be displayed.
Notation
Displays cascade menus for selecting the display notation.
Selected item name
The following items are displayed for selection.
ID, Top Address, Block Size, Total Blocks, Free Blocks
DEC
Displays value in signed decimal number.
HEX
Displays value in hexadecimal number.

(2) Footer row
Jump to Memory (Top Address)
Opens the Memory panel, and displays the contents of the fixed-sized memory pool.
Reset Display Item
Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).