Windows/panels/dialog boxes for debugging are listed below.
| 
 Controls the program execution. Various windows, panels and dialogs can be opened from this window.  | 
|
| 
 Selects a core (PE) to be debugged and displays the core status.  | 
|
| 
 Displays detailed information on the debug tool currently selected in the Project Tree panel, and enables the settings of the tool to be changed.  | 
|
| 
 Displays the results of memory value disassemble and is used to execute line assemble and instruction level debug.  | 
|
| 
 Displays the contents of CPU registers, and modifies register values.  | 
|
| 
 Displays detailed information on set events, switches the events between enabled and disabled, or deletes them.  | 
|
| 
 Displays messages output from the build tool/debug tool/plug-ins, or the results of batch searches carried out using the Find and Replace dialog box.  | 
|
| 
 Selects files to be downloaded and sets the download conditions.  | 
|
| 
 Specifies the number of view columns of memory values on the Memory panel.  | 
|
| 
 Specifies an offset value for the address display on the Memory panel.  | 
|
| 
 Sets the address range to print the contents of the Disassemble panel.  | 
|
| 
 Displays and modifies detailed information on a Combination Break event  | 
|
| 
 Displays and modifies detailed information on an execution-related event.  | 
|
| 
 Displays and modifies detailed information on an access-related event.  | 
|
| 
 Sets the scroll range for the Memory panel/Disassemble panel.  | 
|
| 
 Saves the settings and other data displayed in the respective windows/panels/dialogs or saves upload data.  | 
|
| 
 Displays the functions that access variables in the form of an orthogonal table.  | 
|
| 
 This panel is central to the functionality of the solution for measuring current consumption.  | 
|
| 
 Current Consumption Measurement Condition Setting dialog box [E2]  | 
 This dialog box is used to set measurement conditions in the Measuring Current Consumption panel [E2][Simulator].  | 
| 
 Current Consumption Measurement Trigger Condition Setting dialog box [E2]  | 
 This dialog box is used to set trigger conditions in the Measuring Current Consumption panel [E2][Simulator].  | 
| 
 Current Consumption Measurement Search dialog box [E2][Simulator]  | 
 This dialog box is used to specify and search the detailed conditions in the Measuring Current Consumption panel [E2][Simulator].  | 
| 
 This dialog box is used to save the values for current in the Measuring Current Consumption panel [E2][Simulator].  | 
|
| 
 This panel is used to configure the virtual target system and operate the virtual components.  | 
| 
 Opens and controls various simulator GUI's windows and dialog boxes.  | 
|
| 
 Setting of loop information for the Signal Data Editor window  | 
|
| 
 Selection of display pins in the Signal Data Editor window and Timing Chart window  | 
|
| 
 Detailed search of the Timing Chart window  | 
|
| 
 Setting of pull-up/pull-down resistor pin connection information  | 
|
| 
 Setting of connection information for figure, character, and bitmap pins  | 
|
| 
 List display of object pin connection status in the I/O Panel window  | 
|