Everything
 

Serial window


This window is used to communicate with the serial interface provided in the CPU.

Since this window operates as the serial interface of the remote node of the CPU, transmission data from CPU turns into reception data in this window, and transmission data from this window turns into reception data in the CPU.

The following two types of files can be handled in this window.

The transmission/reception data displayed in the top area in this window can be saved to the serial log data file (*.log) (CSV format) by selecting the [File] menu >> [Save]/[Save As...].

Moreover, the transmission data created in the lower part of this window can be saved to the serial transmission data file (*.ser) (CSV format) by clicking the [Save] button (the contents can be restored by clicking the [Load] button).

Saving/restoring the created data can also be performed by saving/loading the project file. In this case, however, data is not saved as a CSV format text file but saved into the project file.

Caution 1.

If the saved serial transmission data file is opened or the project file is opened while Simulator GUI is running with a microcontroller different from the one used when the file was created, the settings of the serial interface that are not provided in the microcontroller will not be restored.

Caution 2.

Multiple instances of this window can be opened. After opening this window, select the serial interface to be verified in the Serial selection area.

Figure A.96

Serial Window

 

This section describes the following.

[How to open]

-

Click the button.

-

Select [Serial] from the [Simulator] menu.

[Description of each area]

(1)

Serial selection area

Selects the serial interface to be used.

 

Selects the serial interface to be used from the list of provided serial interfaces (drop-down list)Note.

 

Selects the transfer mode (master or slave) when IIC or IICA has been selected from the list of serial interfaces.

 

Selects the time information unit applied to [Wait] in the Serial editor area from the drop-down list.

The time information unit can be changed by selecting the [Edit] menu >> [Time unit].

Note

Once selected, the serial interface cannot be changed.
If you wish to change the serial interface, newly open another Serial window.

(2)

Log display area

Displays the transmission/reception data.

The display timing is when all the bits constituting the data have been received or sent.

Only data from which the start bit, stop bit, and parity bit have been deleted is displayed in this area.

The notation of data can be changed by selecting the [View] menu>> [Numeric Representation] >> [Binary]/[Hexadecimal].

Log display is cleared upon debugger or simulator reset.

Time

Displays the time from the completion of reception/transmission of the previous data until completion of reception/transmission of the current data.

The time information unit is specified by selecting the [Edit] menu >> [Time unit].

Send Data

Displays the data sent by this window (data received by the CPU).

Receive Data

Displays the data received by this window (data sent by the CPU).

Status

Displays the status during data reception.

When an error occurs, one of the following marks is displayed. When everything is normal, nothing is displayed.

P

Parity error (mismatching parity bit)

F

Framing error (stop bit not detected)

(3)

Serial editor area

This area is where the transmission data is created.

This area can be shown or hidden by selecting the [View] menu >> [Serial Editor].

No.

This is a number assigned sequentially from the beginning. It cannot be directly written.

The maximum number is 9,999 lines.

Wait

Specifies the time from the completion of transmission or reception of the immediately previous data until the start of transmission or reception of next data.Valid during transmission using the [Auto send] button and during reception using the [Auto receive] button.

The time information unit is the unit selected by selecting the [Edit] menu >> [Time unit].

The wait value is input by placing the cursor in the Wait field to be edited and double-clicking.

One wait value can be written per operation.

Data

This area is used to edit transmission data.

Data can be directly input by placing the cursor in the data field and double-clicking.

Data suffixed by "0x" is treated as hexadecimal data, and data suffixed by "0b" is treated as binary data. The default code is the hexadecimal code.

If a bit length different from that specified in the Format (UART) dialog box or Format (CSI) dialog box is specified, data from the lower bit is valid.

One data can be written per operation.

Button

Format

Opens the Format (UART) dialog box, Format (CSI) dialog box, or Format (IIC) dialog box.

All Clear

Clears all Serial editor area.

Load

Loads the contents of the previously saved serial transmission data file (*.ser) and restores them in the Serial editor area.

A file created for UART cannot be loaded as a file for CSI and vice versa.

Save

Saves the contents of the Serial editor area to the specified serial transmission data file (*.ser).

Send

Sends one of the data selected in the Serial editor area.

The next data becomes selected upon completion of transmission.

If no data is selected, the first data is sent.

Auto Send

Makes the data selected in the Serial editor area the first data, and automatically transfers from the data to the bottom of the area. The data transmission time interval is the time specified for Wait.

Receive

Note

The [Send] button is switched to [Receive] when this window is used as the reception side of IICA.

Cancels the wait state and starts data reception.

Auto Receive

Note

The [Auto Send] button is switched to [Auto Receive] when this window is used as the reception side of IICA.

Cancels the wait state at time interval specified in the Serial editor area and automatically receives data. The data reception time interval is the time specified for Wait.

Start

This button is activated when IIC or IICA is selected from the list of serial interfaces in the Serial selection area, and master mode is selected as the transfer mode.

Pressing it generates a start condition, which starts serial transfer.

Stop

This button is activated when IIC or IICA is selected from the list of serial interfaces in the Serial selection area, and master mode is selected as the transfer mode.

Pressing it generates a stop condition, which stops serial transfer.

Send Address

This button is activated when IIC or IICA is selected from the list of serial interfaces in the Serial selection area, and master mode is selected as the transfer mode.

Pressing it sends the address of the slave which is to be the other party in communications.

Note

These buttons are disabled when IIC is selected from the list of serial interface types in the Serial selection area.

Caution

The help for this window will not be displayed even if the [F1] key on the keyboard is pressed while the cursor is placed in this area.

Remark

When the CSI selected in this window is set to master mode, the clock must be supplied for reception. To perform reception, transmission of dummy data is therefore required.

[Dedicated menu (Serial window)]

(1)

[Edit] menu

Insert

Inserts a new line immediately before the selected line.

Cut

Cuts the selected range and saves it to the clipboard.

Copy

Copies the selected range and copies it to the clipboard.

Paste

Pastes the contents of the clipboard to the selected location.

Delete

Deletes the selected range.

Time unit

Selects the time unit.

 

main clock

Main clock (default)

usec

Microsecond

msec

Millisecond

Format...

Opens the Format (UART) dialog box, Format (CSI) dialog box, or Format (IIC) dialog box.

(2)

[View] menu

Serial Editor

Selects whether Serial editor area is displayed or not.

Numeric Representation

Changes the notation of the Log display area display method.

 

Binary

Displays binary numbers.

Hexadecimal

Displays hexadecimal numbers.

(3)

[Option] menu

Customize...

Opens the Customize dialog box.

[Context menu]

The following context menus are available in the Serial editor area.

Insert

Inserts a new line immediately before the selected line.

Cut

Cuts the selected range and saves it to the clipboard.

Copy

Copies the selected range and copies it to the clipboard.

Paste

Pastes the contents of the clipboard to the selected location.

Delete

Deletes the selected range.