| [General - Debug] category | 
Use this category to configure general setting relating to debugging.
| 
Figure A.45 | Option Dialog Box ([General - Debug] Category) | 
 
The following items are explained here.
[How to open]
| 
- | From the [Tool] menu, select [Options...]. | 
[Description of each area]
| 
(1) | [Observe downloaded load module files changing] | 
|  | 
Monitors load module files downloaded to the debugging tool for changes.  When there is a change, a message dialog box confirming whether to execute the download is displayed. | 
|  | 
Does not monitor load module files downloaded to the debugging tool for changes (default). | 
| 
(2) | [Add source files automatically (for the "Debug Only" project only)] | 
|  | 
In a debug-dedicated project, when downloading a load module file into the debug tool, source files are automatically added to the project tree (default). | 
|  | 
In a debug-dedicated project, when downloading a load module file into the debug tool, source files are not automatically added to the project tree. | 
| 
Caution | This function is only valid when a load module file has been added to the Download files node of the project tree.When a load module file has been added in the [Download File Settings] tab on the Property panel of the debug tool, source files are not added to the project tree.
 | 
|  | 
Beeps when the execution of a user program is halted due to a break event (hardware or software break). | 
|  | 
Does not beep when the execution of a user program is halted due to a break event (hardware or software break) (default). | 
| 
(4) | [Save the value of SFRs and IORs added in the Watch 4 panel] | 
|  | 
Saves also the states of SFRs and IORs registered in the Watch 4 panel when saving the state of the debug tool.  Note that only the value of SFRs and IORs which can be read or rewritten will be saved. | 
|  | 
Does not save the states of SFRs and IORs registered in the Watch 4 panel when saving the state of the debug tool.  Note that only the value of SFRs and IORs which can be read or rewritten will be saved (default). | 
| 
(5) | [Enable rewind feature] | 
|  | 
Automatically saves the memory and register values just before the debug tool is executed. The saved values can be stored up to the maximum number of times of rewinding. If the maximum number is exceeded, previously saved values will be deleted. | 
|  | 
Does not automatically save the memory and register values just before the debug tool is executed (default). | 
| 
Remark | Saving by the rewind feature is independent of saving of the state of the debug tool. For details on the use of the rewind feature, refer to Saving and Restoring the States of Debug Tools in the User's Manual: Debug Tool. | 
| 
(a) | [Maximum number of times of rewinding] | 
Specify the upper limit for accumulation by the rewind feature.
Either enter a number between 1 and 100 directly via the keyboard, or specify a number via the  buttons.  The default is 50.
 buttons.  The default is 50.
Note that clicking on the [OK] or [Apply] button while this item remains blank causes the tab setting to remain at the previously saved value.
| 
(6) | [Do not distinguish source files with the same file name by the relative path] | 
|  | 
When a source file in a project is associated with a given address and is to be opened in a new panel or shown in front of an existing display if the file has already been displayed in a panel, the relative path to the file is not used. 
Selecting this check box may disable the following operations in some projects. | 
- | Displaying the current PC mark on the Editor panel | 
| 
- | [Go To...] from the context menu on the Editor panel | 
| 
- | Displaying the source text in the Mixed display mode on the Disassemble panel | 
| 
- | [Jump to Source] from the context menu on the Disassemble panel | 
  
Select this check box if you wish to designate source files by their filenames alone. | 
|  | 
When a source file in a project is associated with a given address and is to be opened in a new panel or shown in front of an existing display if the file has already been displayed in a panel, the relative path to the file is used (default). | 
| 
Caution | If you select this check box and there are multiple source files with the same name within a load module, you may not be able to select the correct files. | 
| 
Initialize Settings | 
Returns all currently displayed setting to their default values. | 
[Function buttons]
|  |  | 
| 
Initialize All Settings | 
Restores all settings on this dialog box to their default values. 
Note, however, that newly added items in the [General - External Tools] category will not be removed. | 
| 
OK | 
Applies all setting and closes this dialog box. | 
| 
Cancel | 
Ignores the setting and closes this dialog box. | 
| 
Apply | 
Applies all setting (does not close this dialog box). | 
| 
Help | 
Displays the help of this dialog box. |