Use this category to configure general settings relating to program messages.
![](ProjectOperation_Eng-362.gif)
The following items are explained here.
Select the Message dialog box display level (verbosity) from the following drop-down list.
Regardless of this setting, all messages are displayed in the Output panel.
Use this area to select the format in which to display toolbars on each panel, via the following drop-down list.
Displays the Function Key bar in the Main window (default). |
|
Does not display the Function Key bar in the Main window. |
Resizes the window while displaying areas that were not visible before (default). |
|
Resizes the window without displaying areas that were not visible before. |
Specify the number of tab columns.
Either enter a number between 1 and 16 directly via the keyboard, or specify a number via the
buttons. The default is 8.
Note that clicking on the [OK] or [Apply] button while this item remains blank causes the tab setting to remain at the previously saved value.
When the Editor panel is activated, the file currently being opened is selected in the Project Tree panel (default). |
|
Even if the Editor panel is activated, the file currently being opened is not selected in the Project Tree panel. |
Displays overlay icons for Windows Explorer in the Project Tree panel. |
|
Does not display overlay icons for Windows Explorer in the Project Tree panel (default). |
Use this area to select the location of a close button for a split panel, via the following drop-down list.
Restores all settings on this dialog box to their default values. Note, however, that newly added items in the [General - External Tools] category will not be removed. |
|