Use this category to configure general settings relating to fonts and colors on each panel.
![](ProjectOperation_Eng-381.gif)
The following items are explained here.
Use this area to configure the colors.
Select a location from the list for which the color will be specified.
The relationships between the list items and default color settings are as follows.
This color indicates that the contents of a load module are older than those of the source file in the text editor. |
||||
Warning messages are displayed in this color in the Output panel, file names with warnings are displayed in this color in the Project Tree panel, and this color indicates that the contents of a load module are older than those of the source file in the Editor panelNote 2. |
||||
Error messages are displayed in this color in the Output panel, and file names with errors are displayed in this color in the Project Tree panel. |
||||
The reserved words of your compiler/assembler are displayed in this color in the text editor. |
||||
The reserved words of your compiler/assembler are displayed in this color in the Editor panelNote 2 and Disassemble panel. |
||||
Comments (in the case of a C source file, "/* ... */") are displayed in this color in the text editor. |
||||
Comments (in the case of a C source file, "/* ... */") are displayed in this color in the Editor panelNote 2 and Disassemble panel. |
||||
String literals are displayed in this color in the text editor. |
||||
String literals are displayed in this color in the Editor panelNote 2 and Disassemble panel. |
||||
Control characters are displayed in this color in the text editor. |
||||
Control characters are displayed in this color in the Output panel and Editor panelNote 2. |
||||
Not defined (the default color, and the colors for reserved words, comments, and string literals will be applied) |
The outer frame of the background color for highlighting the current line in the text editor. The current line is highlighted when the [Enable line highlight for current] check box is selected for the [Text Editor - General / Debug] category in the Option dialog box. |
|||
Highlighted areas in plug-in products and the like are displayed in this color and the outer frame of the background color for highlighting the current line in the Editor panelNote 2. |
||||
Values changed via the execution of a user program are displayed in this color in the Memory panel, CPU Register panel, Local Variables panel, SFR panel, Watch panel. |
||||
Values forcibly modified by the user are displayed in this color in the Memory panel, CPU Register panel, Local Variables panel, SFR panel, Watch panel and operators are displayed in this color in the Editor panelNote 2. |
||||
The row with the current PC position is displayed in this color in the text editor. |
||||
The row with the current PC position is displayed in this color in the Editor panelNote 2 and Disassemble panel. |
||||
Not defined (the default color, and the colors for reserved words, comments, and string literals will be applied) |
The line at which a break point is set is displayed in this color in the text editor. |
|||
The line at which a break point is set is displayed in this color in the Editor panelNote 2 and Disassemble panel. |
||||
Areas configured for real-time display updates are shown in this color in the Memory panel and Watch panel. |
||||
Locations that have been read or fetched are displayed in this color in the Trace panel [IECUBE] [Simulator]. |
||||
Locations that have been written are displayed in this color in the Trace panel [IECUBE] [Simulator]. |
||||
Locations that have been read and written are displayed in this color in the Trace panel [IECUBE] [Simulator]. |
||||
Locations that the value has been got from the debug tool is not correct in the Memory panel. |
||||
Not defined (the default color, and the colors for reserved words, comments, and string literals will be applied) |
The line for which code coverage is at 100% is displayed in this color in the text editor. |
|||
The line for which code coverage is at 100% is displayed in this color in the Editor panelNote 2 and Disassemble panel. |
||||
Not defined (the default color, and the colors for reserved words, comments, and string literals will be applied) |
The line for which code coverage is at 1 to 99% is displayed in this color in the text editor. |
|||
The line for which code coverage is at 1 to 99% is displayed in this color in the Editor panelNote 2 and Disassemble panel. |
||||
Not defined (the default color, and the colors for reserved words, comments, and string literals will be applied) |
The line for which code coverage is at 0% (not yet executed) is displayed in this color in the text editor. |
|||
The line for which code coverage is at 0% (not yet executed) is displayed in this color in the Editor panelNote 2 and Disassemble panel. |
||||
Non memory-mapped areas in the Memory panel and filenames in the Project Tree panel that do not actually exist are displayed in this color. |
||||
The [Default] text and background colors depend on the Windows settings of the host computer. Here, we use the Windows defaults, which are black text and white background. |
This setting does not apply to the text editor when the [Enable color settings for text editor] check box is selected. |
Displays items selected via the [Setting place] area using the standard text color. |
|
Displays items selected via the [Setting place] area with a user-defined text color. |
Displays items selected via the [Setting place] area using the standard background color. |
|
Displays items selected via the [Setting place] area with a user-defined background color. |
Enables items for the text editor in the [Setting place] area. This allows you to make individual settings for colors in the text editor regardless of the general settings for panels in CS+. |
|
Disables items for the text editor in the [Setting place] area (default). |
The Edit Colors Dialog Box opens. Specify the text color of the item selected via the [Setting place] area. Note, however, that this button will be disabled if the [Use default color] check box is selected. |
|
The Edit Colors Dialog Box opens. Specify the background color of the item selected via the [Setting place] area. Note, however, that this button will be disabled if the [Use default background color] check box is selected. |
|
Resets the color information for the item selected via the [Setting place] area to the defaults. |
![](ProjectOperation_Eng-422.gif)
Display sample text using the color and font settings from the Color options area.
By default the string "AaBbCc" is shown, but you can type an arbitrary string directly into the text box.
Click the [Font...] button to open the Font Dialog Box and configure the fonts for your text editor.
![](ProjectOperation_Eng-423.gif)
Restores all settings on this dialog box to their default values. Note, however, that newly added items in the [General - External Tools] category will not be removed. |
|