Everything

r_s12adn_groupb_interrupt

Performs processing in response to the group B scan end interrupt.

Remark         This function is called to run interrupt processing for the group B scan end interrupt, which is generated when scanning of the analog inputs allocated to group B is completed.

 

[Syntax]

static void    r_s12adn_groupb_interrupt ( void );

Remark         n is the unit number.

 

[Argument(s)]

None.

 

[Return value]

None.