Everything

R_S12ADn_Get_ValueResult

Gets the result of conversion.

 

[Syntax]

#include       "r_cg_s12ad.h"

void    R_S12ADn_Get_ValueResult ( ad_channel_t channel, uint16_t * const buffer );

Remark         n is the unit number.

 

[Argument(s)]

 

I/O

Argument

Description

I

ad_channel_t channel;

Channel number

ADCHANNEL0                        : Input channel AN000

ADCHANNEL1                        : Input channel AN001

ADCHANNEL2                        : Input channel AN002

ADCHANNEL3                        : Input channel AN003

ADCHANNEL4                        : Input channel AN004

ADCHANNEL5                        : Input channel AN005

ADCHANNEL6                        : Input channel AN006

ADCHANNEL7                        : Input channel AN007

ADCHANNEL8                        : Input channel AN008

ADCHANNEL9                        : Input channel AN009

ADCHANNEL10                     : Input channel AN010

ADCHANNEL11                     : Input channel AN011

ADCHANNEL12                     : Input channel AN012

ADCHANNEL13                     : Input channel AN013

ADCHANNEL14                     : Input channel AN014

ADCHANNEL15                     : Input channel AN015

ADCHANNEL16                     : Input channel AN016

ADCHANNEL17                     : Input channel AN017

ADCHANNEL18                     : Input channel AN018

ADCHANNEL19                     : Input channel AN019

ADCHANNEL20                     : Input channel AN020

ADTEMPSENSOR                  : Extended analog input

                                                   (temperature sensor output)

ADINTERREFVOLT                : Extended analog input

                                                   (internal reference voltage)

O

uint16_t * const buffer;

Pointer to the area where the results of conversion are stored

 

[Return value]

None.