Everything

R_S12ADn_Set_CompareValue

Sets compare level.

 

[Syntax]

void    R_S12ADn_Set_CompareValue ( uint16_t reg_value0, uint16_t reg_value1);

Remark         n is the unit number.

 

[Argument(s)]

I/O

Argument

Description

I

uint16_t reg_value0;

Register value set to the compare revel register 0

I

uint16_t reg_value1;

Register value set to the compare revel register 1

 

[Return value]

None.