Realtime OS Resource Information panel
 | 
  
 This panel displays the resource information (e.g. system information and memory area information) of the RI78V4.
 
 Figure A-1.    Realtime OS Resource Information Panel
 
 The following items are explained here.
 
 -	 From the [Debug] menu, select [Download].
 
 -	 From the [View] menu, select [Realtime OS] >> [Resource Information].
 
 [Description of each area]
 
 This panel has the following tabs:
 
 (2)	 Information display area
 
 This area displays the resource information (e.g. system information and memory area information) of the RI78V4.