[Timer Queue] tab | 
 This tab displays the timer queue information (e.g. Object Type and Number of Objects) of the RI78V4.
 This layer displays the timer queue information (e.g. Object Type and Number of Objects) of the RI78V4.
 The waiting task information (e.g. Task Name and ID) only appears if there are tasks queued in the timer queue.
 Remarks 1.	 If the waiting task information (Task Name, ID, Status, Wait Factor, Wait Data, Time Left, Interrupt, Current Priority, Task Start Address, Current PC) in each cell is double clicked, then Editor panel displays the source file of the task, and the caret moves to the corresponding location.
 2.	 If the waiting task information (Current Task SP) in the cell is double clicked, then Memory panel displays the contents of the task stack, and the caret moves to the corresponding location.
 The cyclic handler information (e.g. Cyclic Handler Name and ID) only appears if there are cyclic handlers queued in the timer queue.
 Remark	 If the cyclic handler information (e.g. Cyclic Handler Name and ID) in each cell is double clicked, then Editor panel displays the source file of the cyclic handler, and the caret moves to the corresponding location.
 The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.