This tab displays the interrupt handler information (e.g. Exception Code and Start Address) of the RI78V4.
 
 Figure A-19.    [Interrupt Handler] Tab
 
 The following items are explained here.
 
 -	 From the [Debug] menu, select [Download].
 
 -	 From the [View] menu, select [Realtime OS] >> [Resource Information].
 
 [Description of each area]
 
 (1)	 Information display area
 
 This area displays the interrupt handler information (e.g. Exception Code and Start Address) of the RI78V4.
 
 This area consists of the following items.
 
 
  
  
    | 
 | 
    
 An icon indicating the interrupt handler of the exception code are shown in the following format.
  
 | 
  
  
    | 
 | 
    
 | 
  
  
  
  
    | 
 | 
    
 The start address of the interrupt handler is shown.
  
 | 
  
  
    | 
 | 
    
 The attributes of the interrupt handler (coding language of interrupt handler and information of allocation for interrupt handler) are shown in the following format.
  
   Coding language  Information of allocation
  
 | 
  
  
    
 [Coding language of interrupt handler]
  
 | 
  
  
    | 
 | 
    
 | 
  
  
    | 
 | 
    
 | 
  
  
    
 [Information of allocation for interrupt handler]
  
 | 
  
  
    | 
 | 
    
 | 
  
  
    | 
 | 
    
 | 
  
 
 The context menu displayed in response to a right mouse click differs as follows depending on the area clicked.
 
 
  
  
    | 
 | 
    
 Displays cascade menus for selecting the header items to display.
  
 | 
  
  
    | 
 | 
    
 | 
    
 The following items are displayed for selection.
  
 Exception Code, Start Address, Attribute
  
 | 
  
  
    | 
 | 
    
 The item in question will be displayed.
  
 | 
  
  
    | 
 | 
    
 The item in question will not be displayed.
  
 | 
  
  
    | 
 | 
    
 Displays cascade menus for selecting the display notation.
  
 | 
  
  
    | 
 | 
    
 | 
    
 The following items are displayed for selection.
  
 Exception Code, Start Address
  
 | 
  
  
    | 
 | 
    
 Displays value in signed decimal number.
  
 | 
  
  
    | 
 | 
    
 Displays value in hexadecimal number.
  
 | 
  
 
 
  
  
    
 Jump to Source (Start Address)
  
 | 
    
 Opens the Editor panel, and displays the source code of the interrupt handler.
  
 | 
  
  
    
 Jump to Disassemble (Start Address)
  
 | 
    
 Opens the Disassemble panel, and displays the results of disassembling the interrupt handler.
  
 | 
  
  
    | 
 | 
    
 Resets the display item (e.g. whether or not to display header items, display notation, display order and display width).
  
 |