Use the CPU Register panel below to display the contents of CPU registers (general and control registers) or change the register values.
Choose [CPU Register] from the [View] menu.
For details on how to read each area and details about their functionality, see the section where the CPU Register panel is described.
![](Debug_RX_E-212.gif)
Following methods of operation are described here.
2.11.2.1 Changing the form in which values are displayed