Use the IOR panel shown below to display I/O register contents or change values.
Choose [IOR] from the [View] menu.
For details on how to read each area and details about their functionality, see the section where the IOR panel is described.
![](Debug_RX_E-224.gif)
Following methods of operation are described here.
2.11.3.1 Searching I/O register
2.11.3.2 Putting the I/O registers in order
2.11.3.3 Changing the form in which values are displayed
2.11.3.4 Changing the contents of I/O registers
2.11.3.5 Displaying and changing I/O register contents during program execution