Use the Local Variables panel shown below to display the contents of local variables and change values.
Choose [Local Variable] from the [View] menu.
To display the content of your desired local variable, select a scope in the scope area.
The Local Variables panel shows local variable names and function names. It also shows parameters to functions as local variables.
For details on how to read each area and details about their functionality, see the section where the Local Variables panel is described.
During program execution, nothing is displayed on this panel. |

Following methods of operation are described here.
2.11.5.1 Changing the form in which values are displayed