Everything
2.3.2 Select color

Select the colors used to distinguish the type of pins (power pins, special pins, unused pins, etc.) whose information is displayed in the Device Top View panel which is opened as described in “2.3 Open Device Top View Panel”.

To select the color to be displayed, click [Device Top View Settings] tab >> [Color] in the Property panel and select the color.

Figure 2.8

Select Color

 

Remark

Select the colors to be displayed for the following eight types of items.

Power pins

Selects the display color for power pins (pins whose use is limited to power).

Special pins

Selects the display color for special pins (pins with specified uses).

Unused pins

Selects the display color for unused pins (dual-use pins with no use set in the Device Pin List panel).

Used pins

Selects the display color for used pins (dual-use pins with a use set in the Device Pin List panel).

Device

Selects the display color of the microcontroller.

Highlight color for a selected pin

Selects the background color of a pin selected in the Device Pin List panel, on the [Pin Number] tab.

Highlight color for macro pins

Selects the background color of pins selected in the Device Pin List panel, on the [Macro] tab.

Highlight color for external peripheral pins

Selects the background color of pins selected in the Device Pin List panel, on the [External Peripheral] tab.