Everything

Flow of Microcontroller System Development

This section describes a flow of system development using CS+.

 

 

Following are the functions of CS+ corresponding to the flow of system development.

 

<Function>

 

<Description>

Code generating function

 

A program to implement peripheral functions built in the microcontroller is generated automatically through an easy operation using GUIs.

 

 

 

Edit function/

Build function

 

The edit function is for editing a program. After completing creation of a program, the built function is used to build the program.

 

 

 

Debugging function

 

This function enables you to debug the object code after downloading it to the target microcontroller.

 

 

 

Analysis function

 

This function helps you improve the execution performance and control the quality of a program by checking the analysis result.