Procedure to Create a Program
![]()

This section describes a procedure to create a program.
Start performing the task after installing CS+.
|
(1) Generate code :Configure the peripheral functions built in the microcontroller you are going to use. After completing configuration, generate the code. |
![]()

|
(2) Coding :Edit the program (Copy and paste the sample program). |
![]()

|
(3) Build :Build the program (If an error occurs, edit the program again). |
![]()

|
(4) Debugging :Debug the program using R0K505111S000BE and E1. |
![]()

|
(5) Writing : Write a program to the microcontroller using E1 |