Overview of the Program
This section describes an overview of the program you will create in this tutorial and Renesas Starter Kit for RX111 (R0K505111S000BE).
1. Overview of the Program
You are going to create a simple program which causes two LEDs flash alternately. See "Description of Sample Program" for details on this program.
Two LEDs flash alternately
2. Overview of Renesas Starter Kit for RX111 (R0K505111S000BE)
The following is an overview of R0K505111S000BE which will be used as a target board.
Please set up the switches as follows.
See "Specifications of R0K505111S000BE" in Appendix for details on R0K505111S000BE.
R0K505111S000BE
Evaluation LED0 : Lights in green when the port B7 (PB7) is LOW.
Evaluation LED1 : Lights in orange when the port A0 (PA0) is LOW.
E1(14pin connector) : Used for on-chip debugging.