This dialog box is used to pack and save the project and this product.
Figure A.34 | Pack Settings Dialog Box |
The following items are explained here.
[How to open]
- | On the Project Tree panel, select the Project node, and then select [Save Project and Development Tools as Package...] from the context menu. |
[Description of each area]
(1) | Pack type selection area |
Select the pack type.
|
Pack project and tools
|
Packs the project and this product (default).
|
|
Pack project only
|
Packs the project only.
|
Specify the location in which to save the project and this product.
Enter the absolute path directly, or click the [Browse...] button, and select the location via the Browse For Folder dialog box.
|
Browse...
|
Browse For Folder dialog box appears.
When a folder is selected, the path is shown in the text box.
|
Remark 1. | Up to 247 characters can be entered in [Place] area. When the input violates any restriction, the following messages are shown. |
|
|
|
|
The folder name including the path is too long. Make it within 247 characters.
|
The folder name is more than 247 characters.
|
|
The folder name is invalid. The following characters cannot be used: :, *, ?, ", <, >, |
|
The folder name with the invalid path is designated. The characters, :, *, ?, ", <, >, |, cannot be used for the file name and folder name.
|
|
The folder name is invalid. Specify a folder other than the project folder.
|
A folder inside the project folder is specified.
|
|
The folder that you will save the project is the same to the project folder. Set another place.
|
The target project folder for packing is in the folder specified as the location to save the project (Example: A project folder is specified as the top folder of the packing target and a folder above the project folder is specified as the location to save the project folder).
|
Remark 2. | When the path name is too long to be shown in the text area,
is displayed. The absolute path pops up when the mouse cursor is hovered over
. |
(3) | [Top folder of pack target] area |
Specify the top folder of the packing target.
Enter the absolute path directly, or click the [Browse...] button, and select the location via the Browse For Folder dialog box.
|
Browse...
|
Browse For Folder dialog box appears.
When a folder is selected, the path is shown in the text box.
|
|
|
|
|
The folder name including the path is too long. Make it within 247 characters.
|
The folder name is more than 247 characters.
|
|
The folder name is invalid. The following characters cannot be used: :, *, ?, ", <, >, |
|
The folder name with the invalid path is designated. The characters, :, *, ?, ", <, >, |, cannot be used for the file name and folder name.
|
|
Specify a folder that contains the project folder.
|
A folder that does not contain the project folder is specified.
|
Remark 2. | When the path name is too long to be shown in the text area,
is displayed. The absolute path pops up when the mouse cursor is hovered over
. |
[Function buttons]
|
|
|
|
OK
|
Closes this dialog box and packs and saves the project and this product to the designated condition.
|
|
Cancel
|
Cancels the designated condition and closes the dialog box.
|
|
Help
|
Displays the help of this dialog box.
|