Filter Settings dialog box |
This dialog box sets filter conditions on analysis information which is displayed as the CPU usage status, in the Analysis information table area on the Analysis Result panel.
- Click on
icon in the column header in the Analysis information table area on the Analysis Result panel. From the displayed menu, select [(Custom)].
Sets the logic condition that "both filter conditions set in the 1st filter condition setting area and 2nd filter condition setting area are satisfied".
Sets the logic condition that "either of the filter conditions set in the 1st filter condition setting area and 2nd filter condition setting area is satisfied".
Filters the analysis information to be displayed in the Analysis information table area on the Analysis Result panel, according to the filter condition set in this dialog box.
|
|