Everything

2.4.1 On/Off of item display

On the Analysis Result panel, using the button located in the upper left corner of the Analysis information table area, the user can select types of items to be displayed as a CPU usage status in the table area.
To display or not to display a given item, use the Column Chooser dialog box that is opened by pressing the button located in the upper left corner of the Analysis information table area.
Figure 2-3. Column Chooser Dialog Box
Remarks 1. Whether a given item is or is not to be displayed is specified by clicking on the applicable check box.
Checked
Not checked

2. Pressing the [Default] button in the Column Chooser dialog box resets the item types and their sorting order displayed in the Analysis information table area on the Analysis Result panel to their default condition.