Everything
2.6.2 Change the order of the columns to display

You can change the display order of the items (columns) displayed on the Function List panel/Variable List panel. There are two ways to perform this operation, as shown below.

There are two ways to perform this operation, as shown below.

 

(1)Performing the operation from the panel

(2)Performing the operation from the Column Chooser dialog box

(1)

Performing the operation from the panel

Use the mouse to drag and drop the column name to move directly to an arbitrary column (header area).

Figure 2.13

Change the Order of Displayed Items (Operation from Panel)

(2)

Performing the operation from the Column Chooser dialog box

On the left edge of the panel's header area, click the button to open the Column Chooser dialog box, and then drag and drop the column names to move directly to the desired column (header area) on the panel using the mouse.

Figure 2.14

Change the Order of Displayed Items (Operation from Column Chooser Dialog Box)