Everything
2.5 Options

This section explains CcnvCA78K0 options.

 

-

Uppercase characters and lowercase characters are distinguished for options.

-

When a file name is specified as a parameter, it can include the path (absolute path or relative path). When a file name without the path or a relative path is specified, the reference point of the path is the current folder.

-

When a parameter includes a space (such as a path name), enclose the parameter in a pair of double quotation marks (").

 

Table 2.2

Options

Option

Description

-V

This option displays the version information of CcnvCA78K0.

-h

This option displays the descriptions of CcnvCA78K0 options.

-c

This option specifies the Japanese character code.

-l

This option specifies the list file name.

-o

This option specifies the output file name.

-r

This option specifies where the message is to be output.

-A

This option performs conversion with the functions related to the ANSI standard enabled.