This option displays the descriptions of CcnvCA78K0 options.
[Specification format]
- | Interpretation when omitted |
The descriptions of CcnvCA78K0 options are not displayed.
[Detailed description]
- | This option outputs the descriptions of CcnvCA78K0 options to the standard error output. |
- | Conversion is not performed when this option is specified. |
- | When this option is specified simultaneously with another option, the other option is ignored. |
- | When this option is specified simultaneously with the -V option, the -V option is given priority. |
[Example of use]