This option displays the version information of CcnvCA78K0.
[Specification format]
- | Interpretation when omitted |
The version information of CcnvCA78K0 is not displayed.
[Detailed description]
- | This option outputs the version information of CcnvCA78K0 to the standard error output. |
- | Conversion is not performed when this option is specified. |
- | When this option is specified simultaneously with another option, the other option is ignored. |
[Example of use]