R_PICn_Timer_SyncStart
Generates start triggers of the timers for which simultaneous start is enabled.
[Syntax]
void R_PICn_Timer_SyncStart ( void );
Remark
n is the unit number.
[Argument(s)]
None.
[Return value]