Everything
3.2.18 Peripheral Interconnection

Below is a list of API functions output by the Code Generator for peripheral interconnection use.

Table 3.18

API Functions: [Peripheral interconnection]

API Function Name

Function

R_PICn_Create

Performs initialization necessary to control the peripheral interconnection functions.

R_PICn_Create_UserInit

Performs user-defined initialization relating to the peripheral interconnection functions.

R_PICn_Timer_SyncStart

Generates start triggers of the timers for which simultaneous start is enabled.