Starts SCI3 data transmission by multiprocessor mode.
This API function repeats the byte-level SCI3 transmission from the buffer specified in argument tx_buf the number of times specified in argument tx_num. |
R_SCI3m_Start must be called before this API function is called. |
#include "r_cg_macrodriver.h" MD_STATUS R_SCI3m_Multiprocessor_Send( const uint8_t * tx_buf, uint16_t tx_num, uint8_t rx_id); |