Everything
3.2.9 Serial Communication Interface 3

Below is a list of API functions output by the Code Generator for serial communication interface 3 use.

Table 3.9

API Functions: [Serial communication interface 3]

API Function Name

Function

R_SCI3m_Create

Performs initialization necessary to control the serial communication interface 3 functions.

R_SCI3m_Create_UserInit

Performs user-defined initialization relating to the serial communication interface 3 functions.

r_sci3m_interrupt_receive

Performs processing in response to the SCI reception interrupt.

r_sci3m_interrupt_error

Performs processing in response to the SCI error interrupt.

r_sci3m_interrupt_send

Performs processing in response to the SCI transmit interrupt.

r_sci3m_interrupt_sendend

Performs processing in response to the SCI transmit end interrupt.

r_sci3m_callback_receiveend

Performs processing in response to the SCI reception interrupt.

r_sci3m_callback_sendend

Performs processing in response to the SCI transmit end interrupt.

r_sci3m_callback_error

Performs processing in response to the SCI error interrupt.

R_SCI3m_Start

Sets SCI communication to standby mode.

R_SCI3m_Stop

Ends SCI3 communication.

R_SCI3m_Send

Starts SCI3 data transmission.

R_SCI3m_Receive

Starts SCI3 data reception.

R_SCI3m_Multiprocessor_Send

Starts SCI3 data transmission by multiprocessor mode.

R_SCI3m_Multiprocessor_Receive

Starts SCI3 data reception by multiprocessor mode.