The Code Generator has the following windows, panels and dialog boxes.
This is the first window to open when CS+ is launched. This window is used to operate various components (design tool, build tool, etc.) provided by CS+. |
|
This panel displays the components of the project (microcontroller, design tool, build tool, etc.) in a tree structure. |
|
This panel allows you to view the information on and change the setting for the node selected in the Project Tree panel. |
|
This panel allows you to configure the information necessary to control the peripheral functions (clock generator, port functions, etc.) provided. |
|
This panel allows you to confirm the source code in accord with the settings of the Peripheral Functions panel. |
|
This panel displays operation logs for various components (design tool, build tool, etc.) provided by CS+. |
|