CHAPTER 21 CONFIGURATOR cfg600px
To build systems (load module) that use functions provided by the RI600PX, the information storing data to be provided for the RI600PX is required.
Since information files are basically enumerations of data, it is possible to describe them with various editors.
Information files, however, do not excel in descriptiveness and readability; therefore substantial time and effort are required when they are described.
To solve this problem, the RI600PX provides a utility tool (configurator "cfg600px") that converts a system configuration file which excels in descriptiveness and readability into information files.
The cfg600px reads the system configuration file as a input file, and then outputs information files.
- System information header file (kernel_id.h)
An information file that contains the correspondence between object names (task names, semaphore names, or the like) described in the system configuration file and IDs.
An information file that contains the correspondence between object names (task names, semaphore names, or the like) described in the system configuration file and IDs.
- Service call definition file (kernel_sysint.h)
The declaration for issuing service calls by using INT instruction is described in this file. This file is included by kernel.h.
The declaration for issuing service calls by using INT instruction is described in this file. This file is included by kernel.h.
- ROM definition file (kernel_rom.h), RAM definition file (kernel_ram.h)
These files contain the RI600PX management data. These files must be included only by the boot processing file. For details, refer to "17.2 Boot Processing File (User-Own Coding Module)".
These files contain the RI600PX management data. These files must be included only by the boot processing file. For details, refer to "17.2 Boot Processing File (User-Own Coding Module)".
- System definition file (ri600.inc)
The system definition file is included by the table file (ritable.src) which is generated by the mktitbl.
The system definition file is included by the table file (ritable.src) which is generated by the mktitbl.
- CMT timer definition file (ri_cmt.h)
When either of CMT0, CMT1, CMT or CMT3 is specified for Selection of timer channel for base clock (timer) for in Base Clock Interrupt Information (clock), the Template file (template) is retrieved from the folder indicated by the environment variable "LIB600", and the retrieved file is output after it is renamed to "ri_cmt.h". The CMT timer definition file is used for the base clock timer initialization routine. For details, refer to "10.9 Base Clock Timer Initialization Routine (_RI_init_cmt_knl( ))".
When either of CMT0, CMT1, CMT or CMT3 is specified for Selection of timer channel for base clock (timer) for in Base Clock Interrupt Information (clock), the Template file (template) is retrieved from the folder indicated by the environment variable "LIB600", and the retrieved file is output after it is renamed to "ri_cmt.h". The CMT timer definition file is used for the base clock timer initialization routine. For details, refer to "10.9 Base Clock Timer Initialization Routine (_RI_init_cmt_knl( ))".
Note that, in the examples below, "C>" indicates the command prompt, "D" indicates pressing of the space key, and "<Enter>" indicates pressing of the enter key.
- -U
When an undefined interrupt occurs, the system down is caused. When -U option is specified, the vector number will be transferred to the system down routine (refer to "CHAPTER 15 SYSTEM DOWN"). This is useful for debugging. However, the kernel code size increases by about 1.5 kB.
When an undefined interrupt occurs, the system down is caused. When -U option is specified, the vector number will be transferred to the system down routine (refer to "CHAPTER 15 SYSTEM DOWN"). This is useful for debugging. However, the kernel code size increases by about 1.5 kB.
- file
Specifies the system configuration file name to be input. If the filename extension is omitted, the extension ".cfg" is assumed.
Specifies the system configuration file name to be input. If the filename extension is omitted, the extension ".cfg" is assumed.
Note <ri_root> indicates the installation folder of RI600PX.
The default folder is C:¥Program Files¥Renesas Electronics¥CubeSuite+¥RI600PX.
The default folder is C:¥Program Files¥Renesas Electronics¥CubeSuite+¥RI600PX.
This is started when CubeSuite+ performs a build, in accordance with the setting on the Property panel, on the [System Configuration File Related Information] tab.