CHAPTER 11 SYSTEM STATE MANAGEMENT FUNCTIONS
The RI600PX's system status management function provides functions for referencing the system status such as the context type and CPU lock status, as well as functions for manipulating the system status such as ready queue rotation, scheduler activation, or the like.
Note, refer to "CHAPTER 15 SYSTEM DOWN" for system down (vsys_dwn, ivsys_dwn) and refer to "CHAPTER 17 SYSTEM INITIALIZATION" for starting of the RI600PX (vsta_knl, ivsta_knl).
- rot_rdq, irot_rdq
This service call re-queues the first task of the ready queue corresponding to the priority specified by parameter tskpri to the end of the queue to change the task execution order explicitly.
The following shows the status transition when this service call is used.
This service call re-queues the first task of the ready queue corresponding to the priority specified by parameter tskpri to the end of the queue to change the task execution order explicitly.
The following shows the status transition when this service call is used.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600px*/ #pragma cychandler Cychdr1 /*refer to note 5*/ void Cychdr1 (VP_INT exinf); /*refer to note 5*/ void Cychdr1 (VP_INT exinf) /*Cyclic handler*/ { PRI tskpri = 8; /*Declares and initializes variable*/ /* ......... */ irot_rdq (tskpri); /*Rotate task precedence*/ /* ......... */ return; /*Terminate cyclic handler*/ } |
Note 1 This service call does not perform queuing of rotation requests. If no task is queued to the ready queue corresponding to the relevant priority, therefore, no processing is performed but it is not handled as an error.
Note 2 Round-robin scheduling can be implemented by issuing this service call via a cyclic handler in a constant cycle.
Note 3 The ready queue is a hash table that uses priority as the key, and tasks that have entered an executable state (READY state or RUNNING state) are queued in FIFO order.
Therefore, the scheduler realizes the RI600PX's scheduling system by executing task detection processing from the highest priority level of the ready queue upon activation, and upon detection of queued tasks, giving the CPU use right to the first task of the proper priority level.
Therefore, the scheduler realizes the RI600PX's scheduling system by executing task detection processing from the highest priority level of the ready queue upon activation, and upon detection of queued tasks, giving the CPU use right to the first task of the proper priority level.
Note 4 When TPRI_SELF is specified as tskpri, the base priority of the invoking task is applied as the target priority of this service call.
As for a task which has locked mutexes, the current priority might be different from the base priority. In this case, even if the task issues this servie call specifying TPRI_SELF as parameter tskpri, the ready queue of the current priority that the invoking task belongs cannot be changed.
As for a task which has locked mutexes, the current priority might be different from the base priority. In this case, even if the task issues this servie call specifying TPRI_SELF as parameter tskpri, the ready queue of the current priority that the invoking task belongs cannot be changed.
Note 5 These statements are unnecessary for the cyclic handler which is created by the system configuration file because the cfg600px generates these statement into the "kernel_id.h".
A RUNNING-state task is referenced by issuing the following service call from the processing program.
- get_tid, iget_tid
These service calls store the ID of a task in the RUNNING state in the area specified by parameter p_tskid.
The following describes an example for coding these service calls.
These service calls store the ID of a task in the RUNNING state in the area specified by parameter p_tskid.
The following describes an example for coding these service calls.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600px*/ void Inthdr (void) /*Interrupt handler*/ { ID p_tskid; /*Declares variable*/ /* ......... */ iget_tid (&p_tskid); /*Reference task ID in the RUNNING state*/ /* ......... */ return; /*Terminate interrupt handler*/ } |
Note This service call stores TSK_NONE in the area specified by parameter p_tskid if no tasks that have entered the RUNNING state exist.
In the CPU locked state, the task scheduling is prohibited, and kernel interrupts are masked. Therefore, exclusive processing can be achieved for all processing programs except non-kernel interrupt handlers.
- loc_cpu, iloc_cpu
These service calls transit the system to the CPU locked state.
The service calls that can be issued in the CPU locked state are limited to the one listed below.
These service calls transit the system to the CPU locked state.
The service calls that can be issued in the CPU locked state are limited to the one listed below.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600px*/ #pragma task Task1 /*Refer to note 7*/ void Task1 (VP_INT exinf); /*Refer to note 7*/ void Task1 (VP_INT exinf) { /* ......... */ loc_cpu (); /*Lock the CPU*/ /* ......... */ /*CPU locked state*/ unl_cpu (); /*Unlock the CPU*/ /* ......... */ } |
Note 1 The CPU locked state changed by issuing loc_cpu or iloc_cpu must be cancelled before the processing program that issued this service call ends.
Note 2 The loc_cpu and iloc_cpu do not perform queuing of lock requests. If the system is in the CPU locked state, therefore, no processing is performed but it is not handled as an error.
Note 3 The unl_cpu and iunl_cpu do not perform queuing of unlock requests. If the system is in the CPU unlocked state, therefore, no processing is performed but it is not handled as an error
Note 4 The unl_cpu and iunl_cpu do not cancel the dispatching disabled state that was set by issuing dis_dsp.
Note 5 The base clock interrupt is masked during the CPU locked state. Therefore, time handled by the TIME MANAGEMENT FUNCTIONS may be delayed if the period of the CPU locked state becomes long.
Note 7 These statements are unnecessary for the task which is created by the system configuration file because the cfg600px generates these statement into the "kernel_id.h".
It may be necessary to refer to current CPU locked state in functions that are called from two or more tasks and handlers. In this case, sns_loc is useful.
- sns_loc
This service call examines whether the system is in the CPU locked state or not. This service call returns TRUE when the system is in the CPU locked state, and return FALSE when the system is in the CPU unlocked state.
The following describes an example for coding this service call.
This service call examines whether the system is in the CPU locked state or not. This service call returns TRUE when the system is in the CPU locked state, and return FALSE when the system is in the CPU unlocked state.
The following describes an example for coding this service call.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600px*/ void CommonFunc ( void ); void CommonFunc ( void ) { BOOL ercd; /*Declares variable*/ /* ......... */ ercd = sns_loc (); /*Reference CPU state*/ if (ercd == TRUE) { /* ......... */ /*CPU locked state*/ } else if (ercd == FALSE) { /* ......... */ /*CPU unlocked state*/ } /* ......... */ } |
In the dispatching disabled state, the task scheduling is prohibited. Therefore, exclusive processing can be achieved for all tasks.
The following service call moves to the dispatching disabled state. And also when PSW.IPL is changed to other than 0 by using chg_ims, the system shifts to the dispatching disabled state.
The dispatching disabled state is cancelled by the following service call, ext_tsk, exd_tsk and chg_ims that changes PSW.IPL to 0.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600px*/ #pragma task Task1 /*Refer to note 5*/ void Task1 (VP_INT exinf); /*Refer to note 5*/ void Task1 (VP_INT exinf) { /* ......... */ dis_dsp (); /*Disable dispatching*/ /* ......... */ /*Dispatching disabled state*/ ena_dsp (); /*Enable dispatching*/ /* ......... */ } |
Note 1 The dispatching disabled state must be cancelled before the task that issued dis_dsp moves to the DORMANT state.
Note 2 The dis_dsp does not perform queuing of lock requests. If the system is in the dispatching disabled state, therefore, no processing is performed but it is not handled as an error.
Note 3 The ena_dsp does not perform queuing of unlock requests. If the system is in the dispatching enabled state, therefore, no processing is performed but it is not handled as an error
Note 4 If a service call (such as wai_sem, wai_flg) that may move the status of the invoking task is issued while the dispatching disabled state, that service call returns E_CTX regardless of whether the required condition is immediately satisfied.
Note 5 These statements are unnecessary for the task which is created by the system configuration file because the cfg600px generates these statement into the "kernel_id.h".
It may be necessary to refer to current dispatching disabled state in functions that are called from two or more tasks . In this case, sns_dsp is useful.
- sns_dsp
This service call examines whether the system is in the dispatching disabled state or not. This service call returns TRUE when the system is in the dispatching disabled state, and return FALSE when the system is in the dispatching enabled state.
The following describes an example for coding this service call.
This service call examines whether the system is in the dispatching disabled state or not. This service call returns TRUE when the system is in the dispatching disabled state, and return FALSE when the system is in the dispatching enabled state.
The following describes an example for coding this service call.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600px*/ void CommonFunc ( void ); void CommonFunc ( void ) { BOOL ercd; /*Declares variable*/ /* ......... */ ercd = sns_dsp (); /*Reference dispatching state*/ if (ercd == TRUE) { /* ......... */ /*Dispatching disabled state*/ } else if (ercd == FALSE) { /* ......... */ /*Dispatching enabled state*/ } /* ......... */ } |
It may be necessary to refer to current context type in functions that are called from two or more tasks and handlers. In this case, sns_ctx is useful.
- sns_ctx
This service call examines the context type of the processing program that issues this service call. This service call returns TRUE when the processing program is non-task context, and return FALSE when the processing program is task context.
The following describes an example for coding this service call.
This service call examines the context type of the processing program that issues this service call. This service call returns TRUE when the processing program is non-task context, and return FALSE when the processing program is task context.
The following describes an example for coding this service call.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600px*/ void CommonFunc ( void ); void CommonFunc ( void ) { BOOL ercd; /*Declares variable*/ /* ......... */ ercd = sns_ctx ( ); /*Reference context type*/ if (ercd == TRUE) { /* ......... */ /*Non-task contexts*/ } else if (ercd == FALSE) { /* ......... */ /*Task contexts*/ } /* ......... */ } |
It may be necessary to refer to current dispatch pending state in functions that are called from two or more tasks and handlers. In this case, sns_dpn is useful.
- sns_dpn
This service call examines whether the system is in the dispatch pending state or not. This service call returns TRUE when the system is in the dispatch pending state, and return FALSE when the system is not in the dispatch pending state.
The following describes an example for coding this service call.
This service call examines whether the system is in the dispatch pending state or not. This service call returns TRUE when the system is in the dispatch pending state, and return FALSE when the system is not in the dispatch pending state.
The following describes an example for coding this service call.
#include "kernel.h" /*Standard header file definition*/ #include "kernel_id.h" /*Header file generated by cfg600px*/ void CommonFunc ( void ); void CommonFunc ( void ) { BOOL ercd; /*Declares variable*/ /* ......... */ ercd = sns_dpn (); /*Reference dispatch pending state*/ if (ercd == TRUE) { /* ......... */ /*Dispatch pending state*/ } else if (ercd == FALSE) { /* ......... */ /*Other state*/ } /* ......... */ } |