Everything

 

-insert_dbtag_with_label [V1.06.00 or later]


This option controls insertion of the dbtag instruction.

[Specification format]

-insert_dbtag_with_label=file, line, label, tagid

 

-

Interpretation when omitted

The dbtag instruction is not inserted.

[Detailed description]

-

This option inserts a local label and dbtag instruction at the specified location, based on the information for source debugging.

-

When this option is specified, the -g option also becomes valid at the same time.

-

This function is assumed to be used via CS+ and it should not be used directly by the user.