This option generates an instruction string that performs a misaligned memory access.
For memory accesses, this option generates a more effective instruction string assuming that the device supports access to unaligned addresses. |
Specifying this option more than once has the same effect as specifying it once only. No warning is output in this case. |