Everything

 

-MSg_unused


This option notifies the user of the external defined symbol that is not referenced.

[Specification format]

-MSg_unused

 

-

Interpretation when omitted

None

[Detailed description]

-

This option notifies the user of the external defined symbol that is not referenced during link processing through an output message.

[Example of use]

-

To notify the user of the external defined symbol that is not referenced, describe as:

>rlink a.obj b.obj -message -msg_unused

[Remark]

-

If a load module file is input, this option will be invalid.

-

This option must be specified together with the -message option.

-

The a message may be output for the function that inline expansion was performed during compilation.
In this case, add a static declaration for the function definition to suppress the output of the message.

-

If there are references to constant symbols within the same file, references are not correctly analyzed so that information notified by the output messages will be incorrect.