This option changes the name of a symbol or section that was input from a library.
-LIB_REName=suboption[, ...] suboption := (names) | file(names) | file|modules(names) modules := module[|module ...] names := name1=name2[, ...] |
This option changes the name of a global symbol or section included in a module within the library that was specified by the -library option. |
Specify the symbol name or section name to be changed as name1. Specify the symbol name or section name after changing as name2. |
If there are two or more files or modules with the same name, the priority depends on the input order. |
If this option is specified together with the -form={object,library}, -extract or -strip option, an error will occur. |
When the -form={absolute|hexadecimal|stype|binary} option is specified, the -show=struct option cannot be specified together. |
Correct operation is not guaranteed if this option is used in combination with the compile option -Omerge_files. |