Everything

 

-EXIt


This option specifies the end of option specifications.

[Specification format]

-EXIt

 

-

Interpretation when omitted

None

[Detailed description]

-

This option specifies the end of option specifications.

[Caution]

-

This option can be used only in a subcommand file.

[Example of use]

-

Create subcommand file "sub.txt" with the following content.

input=a.obj,b.obj                       ;(1)
start=.SEC1,.SEC2,.SEC3/100,.SEC4/8000  ;(2)
output=a.abs                            ;(3)
exit

 

To specify subcommand file sub.txt, describe as:

>rlink -subcommand=sub.txt -nodebug

 

Processing from (1) to (3) are executed and a.abs is output.

The -nodebug option specified on the command line after this option is executed is invalid.