Everything

 

-VERBOSE [V1.10 or later]


This option displays detailed information in the standard error output.

[Specification format]

-VERBOSE=<sub>[, ...]
sub : CRC

 

-

Interpretation when omitted

None

[Detailed description]

-

This option displays the contents specified by the suboption in the standard error output.

-

The suboption below can be specified.

CRC

This suboption displays the CRC operation result and its output address.

Valid when the crc option is specified.

[Example of use]

-

To display the CRC operation result and its output address in the standard error output, describe as:

> rlink a.obj -form=stype -start=.SEC1/1000 -crc=2000=1000-10ff/CCITT -verbose=crc