Everything

-output


This option specifies the output file.

[Specification format]

-output=file

 

-

Interpretation when omitted

A standard library with the file name stdlib.lib is generated in the current folder.

[Detailed description]

-

This option specifies the output file name for the standard library.

-

file should be specified by using an absolute path or a relative path.

-

A relative path used to specify file is interpreted as the relative path from the current folder.

-

An error will occur if file is omitted.