Everything

-logo / -nologo


This option controls the copyright display.

[Specification format]

-logo
-nologo

 

-

Interpretation when omitted

The copyright is displayed.

[Detailed description]

-

When -logo is specified, the copyright is displayed. When -nologo is specified, the copyright is not displayed.

-

If these options are specified at the same time, the option specified last will be valid.