Everything

-lnkcmd


< Compile Options / Assemble and Linkage Options >

[Format]

-lnkcmd=<file name>

[Description]

-

This option specifies the linkage options to pass to rlink with a subcommand file.

[Example]

ccrx -isa=rxv1 -output=abs=tp.abs -lnkcmd=file.sub tp1.c tp2.c

The above description has the same meaning as the following three command lines:

ccrx -isa=rxv1 -output=src tp1.c tp2.c]
asrx -isa=rxv1 tp1.src tp2.src
rlink -subcommand=file.sub -form=abs -output=tp tp1.obj tp2.obj

[Remarks]

-

If this option is specified for more than one time, all specified subcommand files are valid.

-

Refer to the -subcommand option of the optimizing linkage editor for the contents of the subcommand file passed to the -lnkcmd option.