Everything

-asmopt


< Compile Options / Assemble and Linkage Options >

[Format]

-asmopt=["]<assembler option>["]

[Description]

-

This option specifies the assembler options to pass to asrx with a string.

-

Multiple options can be specified by enclosing them with double-quote marks (").

[Example]

ccrx -isa=rxv1 -asmopt="-chkpm" sample.c

The above description has the same meaning as the following two command lines:

ccrx -isa=rxv1 -output=src sample.c
asrx -isa=rxv1 -chkpm sample.src

[Remarks]

-

If this option is specified for more than one time, all specified assembler options are valid.