Everything

-lnkopt


< Compile Options / Assemble and Linkage Options >

[Format]

-lnkopt=["]<linkage option>["]

[Description]

-

This option specifies the linkage options to pass to rlink with a string.

-

Multiple options can be specified by enclosing them with double-quote marks (").

[Example]

ccrx -isa=rxv1 -output=abs=tp.abs -lnkopt="-start=P,C,D/100,B/8000" tp1.c tp2.c

The above description has the same meaning as the following three command lines:

ccrx -isa=rxv1 -output=src tp1.c tp2.c
asrx -isa=rxv1 tp1.src tp2.src
rlink -start=P,C,D/100,B/8000 -form=abs -output=tp tp1.obj tp2.obj

[Remarks]

-

If this option is specified for more than one time, all specified linkage options are valid.

-

A single -lnkopt option can only take a single linkage option. To pass multiple linkage options, specify -lnkopt options as many times as the number of linkage options you require.